MCF52233 Ethernet Autonegotiation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52233 Ethernet Autonegotiation

469 Views
IRTrans
Contributor III

Hi,

we are working on a project based on the MCF52233. We are using the FNET IP Stack.

 

We are already using our own HW. Everything ist working fine, however the Ethernet Autonegotiation does not work correctly. We do get a link but only 10MBit  / Half Duplex. The "Auto-Negotiation Complete bit" (ACOMP) in the MII Status register is never set. Nevertheless a 10MBit Half Duplex connection is established. With manual parameters we can get 100 MBit FDX.

 

Apart from the FNET code I have tried the PHY init code used in the Coldfire TCP Lite stack, however the problem is the same.

 

We are using a MCF52233 with mask version 3M23E - this version is no longer affected by the common Autonegotiation bug.

 

Does anybody have working code for the Autonegotiation?

Has anybody used Autonegotiation on the MCF52233/52235 at all?

 

Thanks in advance, Marcus

Labels (1)
0 Kudos
2 Replies

290 Views
butok
NXP Employee
NXP Employee

Hi Marcus,

>>We are using a MCF52233 with mask version 3M23E -

>> this version is no longer affected by the common Autonegotiation bug.

How do you know that it is not affected by the auto-negotiation bug? Do you have a test code that can prove it?

Thanks,

Andrey

0 Kudos

290 Views
IRTrans
Contributor III

At least the Errata says the the 3M23E mask version is no longer affected by the bug ...

Marcus

0 Kudos