MCF5223: using of CFM command to write a really big array in flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5223: using of CFM command to write a really big array in flash

2,640件の閲覧回数
sev
Contributor I
Hi,
 
I use the CFM module to copy  128 char arrays (a file dowloaded throw the UART) into the flash by using the back door.
However, After several copy in flash, the process speed become really low.
 
has anybody any idea on the reason ?
 
Really thanks for your help.
Sév
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,053件の閲覧回数
Kremer
Contributor I
Are you really waiting for it to finish write the current data?

while( !(MCF_CFM_CFMUSTAT & MCF_CFM_CFMUSTAT_CCIF));

I´ve did an ehternet bootloader using the CFM fro internal flash reprogram and never faced this behavior you mentioned.
0 件の賞賛
返信

1,053件の閲覧回数
doublev724
Contributor I

Hi Kremer

 

Did you use RTCS for ethernet and write new image to flash througth CFM commands?

 

I am working a similar project and find the "while( !(MCF_CFM_CFMUSTAT & MCF_CFM_CFMUSTAT_CCIF));" never returns. Did you get similar issues?

 

song

0 件の賞賛
返信