MCF52223 ADC's SYNCA signal confusion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52223 ADC's SYNCA signal confusion

1,264件の閲覧回数
Harjit
Contributor II

I'm looking at using the MCF52223 and wanted to use a timer to kick of a set of ADC conversions.

 

The MCF52223 datasheets, ADC chapter block diagram shows a SYNCx signal and then the description says that a conversion can be initiated by asserting a positive edge on SYNC0 input.

 

If I search for SYNC0 there is no such pin. The language makes me believe that this should be a pin.

 

In the signals section, the ADC Signals section talks about ADC Sync Inputs and calls them SYNCA / SYNCB <- huh? what happened to SYNC0?

 

So, for the longest time, I thought that SYNCA and SYNCB must be the ADC sync inputs until just a few minutes ago, when I came across a SYNCn set of signals in the General Purpose Timer section and this section refers to SYNCA and SYNCB for synchronization of the timer counter.

 

I'd love to know:

* Do the ADCs have sync inputs?

  * If so, what are they called and what are their pin #s for the 100 pin QFP package?

 

Is there updated documentation around this?

 

Thanks,

Harjit

PS: The MCF52223 Reference manual talks about CANTX and CANRX and those don't exist on the MCF52223...

ラベル(1)
0 件の賞賛
返信
1 返信

678件の閲覧回数
MrBean
Contributor I

:smileyvery-happy: Welcome to Freescale documentation !

 

I have not been using the ADC yet, so i dont know the answer.

 

Freescale creates new documetation for new processors by copying for an older processors' docs.

This is then edited to suit the new mcu.

Very often something is forgotten in the editing...

This is then again copied for newer mcus :smileytongue:

 

Look at MCF52211RM.pdf and MCF52235RM.pdf , that will clear up some confusions.

0 件の賞賛
返信