MCF52221 : UART, external interrupt : no detection of external interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52221 : UART, external interrupt : no detection of external interrupt

1,708 次查看
polo
Contributor I
Hi,
I try to use the uart 1 and the the edge port module IRQ1 in input interrupt.
My 2 codes are good separately.
But when I use both then the detection of the IRQ1 functions one time.
The UART functions at 115200bauds and IPL = 2 and all ICR are different, I use asm_set_ipl before before modify all IMR.

Someone can help me?
thanks,
Best regards

Yohan
标签 (1)
0 项奖励
回复
1 回复

772 次查看
mccPaul
Contributor I
Hi
 
You need to post the code that you are using to set up and then reset each interrupt.
 
You must have something wrong.
 
Paul.
0 项奖励
回复