Trying to get a center aligned PWM output working. Managed to get Normal PWM working but when I change to center aligned it wont work. Any suggestions would really help me. I am using the processor expert to generate this code.
void FT1_Init(void)
{
/* SIM_SCGC3: FTM1=1 */
SIM_SCGC3 |= (uint8_t)0x08U;
/* FTM1_MODE: FAULTIE=0,FAULTM=0,CAPTEST=0,PWMSYNC=0,WPDIS=1,INIT=0,FTMEN=1 */
FTM1_MODE = (uint8_t)0x05U;
/* FTM1_SC: TOF=0,TOIE=0,CPWMS=0,CLKS=0,PS=0 */
FTM1_SC = (uint8_t)0x00U;
/* FTM1_C0SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C0SC = (uint8_t)0x00U;
/* FTM1_C1SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C1SC = (uint8_t)0x00U;
/* FTM1_C2SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C2SC = (uint8_t)0x00U;
/* FTM1_C3SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C3SC = (uint8_t)0x00U;
/* FTM1_C4SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C4SC = (uint8_t)0x00U;
/* FTM1_C5SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C5SC = (uint8_t)0x00U;
/* FTM1_CNTINH: INIT_H=0 */
FTM1_CNTINH = (uint8_t)0x00U;
/* FTM1_CNTINL: INIT_L=0 */
FTM1_CNTINL = (uint8_t)0x00U;
/* FTM1_CNTH: COUNT_H=0 */
FTM1_CNTH = (uint8_t)0x00U;
/* FTM1_CNTL: COUNT_L=0 */
FTM1_CNTL = (uint8_t)0x00U;
/* FTM1_MODH: MOD_H=0 */
FTM1_MODH = (uint8_t)0x00U;
/* FTM1_MODL: MOD_L=0x4A */
FTM1_MODL = (uint8_t)0x4AU;
/* FTM1_FILTER0: CHoddFVAL=0,CHevenFVAL=0 */
FTM1_FILTER0 = (uint8_t)0x00U;
/* FTM1_FILTER1: CHoddFVAL=0,CHevenFVAL=0 */
FTM1_FILTER1 = (uint8_t)0x00U;
/* FTM1_C0SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=1,ELSA=0,??=0,DMA=0 */
FTM1_C0SC = (uint8_t)0x08U;
/* FTM1_C1SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=1,ELSA=0,??=0,DMA=0 */
FTM1_C1SC = (uint8_t)0x08U;
/* FTM1_C2SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=1,ELSA=0,??=0,DMA=0 */
FTM1_C2SC = (uint8_t)0x08U;
/* FTM1_C3SC: CHF=0,CHIE=0,MSB=0,MSA=0,ELSB=1,ELSA=0,??=0,DMA=0 */
FTM1_C3SC = (uint8_t)0x08U;
/* FTM1_C4SC: CHF=0,CHIE=0,MSB=0,MSA=1,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C4SC = (uint8_t)0x10U;
/* FTM1_C5SC: CHF=0,CHIE=0,MSB=0,MSA=1,ELSB=0,ELSA=0,??=0,DMA=0 */
FTM1_C5SC = (uint8_t)0x10U;
/* FTM1_C0VH: VAL_H=0 */
FTM1_C0VH = (uint8_t)0x00U;
/* FTM1_C0VL: VAL_L=0x14 */
FTM1_C0VL = (uint8_t)0x14U;
/* FTM1_C1VH: VAL_H=0 */
FTM1_C1VH = (uint8_t)0x00U;
/* FTM1_C1VL: VAL_L=0x14 */
FTM1_C1VL = (uint8_t)0x14U;
/* FTM1_C2VH: VAL_H=0 */
FTM1_C2VH = (uint8_t)0x00U;
/* FTM1_C2VL: VAL_L=0x16 */
FTM1_C2VL = (uint8_t)0x16U;
/* FTM1_C3VH: VAL_H=0 */
FTM1_C3VH = (uint8_t)0x00U;
/* FTM1_C3VL: VAL_L=0x22 */
FTM1_C3VL = (uint8_t)0x22U;
/* FTM1_C4VH: VAL_H=0 */
FTM1_C4VH = (uint8_t)0x00U;
/* FTM1_C4VL: VAL_L=0 */
FTM1_C4VL = (uint8_t)0x00U;
/* FTM1_C5VH: VAL_H=0 */
FTM1_C5VH = (uint8_t)0x00U;
/* FTM1_C5VL: VAL_L=0 */
FTM1_C5VL = (uint8_t)0x00U;
/* FTM1_POL: POL7=0,POL6=0,POL5=0,POL4=0,POL3=0,POL2=0,POL1=0,POL0=0 */
FTM1_POL = (uint8_t)0xFFU;
/* FTM1_OUTINIT: CH7OI=0,CH6OI=0,CH5OI=0,CH4OI=0,CH3OI=0,CH2OI=1,CH1OI=0,CH0OI=1 */
FTM1_OUTINIT = (uint8_t)0x05U;
/* FTM1_OUTMASK: CH7OM=0,CH6OM=0,CH5OM=0,CH4OM=0,CH3OM=0,CH2OM=0,CH1OM=0,CH0OM=1 */
FTM1_OUTMASK = (uint8_t)0x01U;
/* FTM1_COMBINE0: ??=0,FAULTEN=0,SYNCEN=0,DTEN=0,DECAP=0,DECAPEN=0,COMP=0,COMBINE=0 */
FTM1_COMBINE0 = (uint8_t)0x00U;
/* FTM1_COMBINE1: ??=0,FAULTEN=0,SYNCEN=0,DTEN=0,DECAP=0,DECAPEN=0,COMP=0,COMBINE=0 */
FTM1_COMBINE1 = (uint8_t)0x00U;
/* FTM1_COMBINE2: ??=0,FAULTEN=0,SYNCEN=0,DTEN=0,DECAP=0,DECAPEN=0,COMP=0,COMBINE=0 */
FTM1_COMBINE2 = (uint8_t)0x00U;
/* FTM1_DEADTIME: DTPS=0,DTVAL=0 */
FTM1_DEADTIME = (uint8_t)0x00U;
/* FTM1_SYNC: SWSYNC=0,TRIG2=0,TRIG1=0,TRIG0=0,SYNCHOM=0,REINIT=0,CNTMAX=0,CNTMIN=0 */
FTM1_SYNC = (uint8_t)0x00U;
/* FTM1_EXTTRIG: TRIGF=0,INITTRIGEN=0,CH1TRIG=0,CH0TRIG=0,CH5TRIG=0,CH4TRIG=0,CH3TRIG=0,CH2TRIG=0 */
FTM1_EXTTRIG = (uint8_t)0x00U;
/* FTM1_FLTFILTER: ??=0,??=0,??=0,??=0,FFVAL=0 */
FTM1_FLTFILTER = (uint8_t)0x00U;
/* FTM1_FLTCTRL: FFLTR3EN=0,FFLTR2EN=0,FFLTR1EN=0,FFLTR0EN=0,FAULT3EN=0,FAULT2EN=0,FAULT1EN=0,FAULT0EN=0 */
FTM1_FLTCTRL = (uint8_t)0x00U;
/* FTM1_MODE: FAULTIE=0,FAULTM=0,CAPTEST=0,PWMSYNC=0,WPDIS=1,INIT=1,FTMEN=1 */
FTM1_MODE = (uint8_t)0x07U;
/* FTM1_SC: TOF=0,TOIE=0,CPWMS=1,CLKS=1,PS=0 */
FTM1_SC = (uint8_t)0x28U;
}
also have this which I don't think is needed
MXC_PTAPF4 = (MXC_PTAPF4 & 0xF) |(0x4 <<4);
MXC_PTAPF3 = 0x4;
Thank you
解決済! 解決策の投稿を見る。
Seems like the problem is that at the end each of the output value registers gets reset to zero. such as
FTM1_C0VL
So wrote this small function which then produces the waveform I wanted
#define FT1_CLK_FQ 20971500
#define DEAD_TIME 5
void StartFMT1(u32 Fq){
u16 Mod = (u16)((20971500/2)/Fq);
FTM1_SC &= ~(BIT4 | BIT3);
// Timer frequency is clk frequency divided by 2*Period
FTM1_MOD = Mod;
FTM1_C0V = Mod/2 + DEAD_TIME;
FTM1_C1V = Mod/2 - DEAD_TIME;
FTM1_C2V = Mod/2;
FTM1_C3V = Mod/2;
// Turn on FT1
FTM1_SC |= BIT3;
}
Seems like the problem is that at the end each of the output value registers gets reset to zero. such as
FTM1_C0VL
So wrote this small function which then produces the waveform I wanted
#define FT1_CLK_FQ 20971500
#define DEAD_TIME 5
void StartFMT1(u32 Fq){
u16 Mod = (u16)((20971500/2)/Fq);
FTM1_SC &= ~(BIT4 | BIT3);
// Timer frequency is clk frequency divided by 2*Period
FTM1_MOD = Mod;
FTM1_C0V = Mod/2 + DEAD_TIME;
FTM1_C1V = Mod/2 - DEAD_TIME;
FTM1_C2V = Mod/2;
FTM1_C3V = Mod/2;
// Turn on FT1
FTM1_SC |= BIT3;
}