i intend to implement On-The-Go capability into my USB gateway device which works on Freescale's MCF51JM128.
I am having a little confusion as the LQFP 64 pin package which i'll be using is lacking USB_ID Pin(pin#40 pin of LQFP80).Henceforth, how should i proceed in realizing OTG in my device?
Also, i am using the CMX stack, what changes do i need to bring about in the stack? Will it work if i configure any other GPIO pin as USB_ID pin or should i?
please help !
Thanks
DIPIN
Hi All,
No comments from the Experts !?