MCF51JM128, LQFP 64 Package and OTG Confusion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM128, LQFP 64 Package and OTG Confusion

1,057 Views
Dipin
Contributor II

i intend to implement On-The-Go capability into my USB gateway device which works on Freescale's MCF51JM128.

I am having a little confusion as the LQFP 64 pin package which i'll be using is lacking USB_ID Pin(pin#40 pin of LQFP80).Henceforth, how should i proceed in realizing OTG in my device?

Also, i am using the CMX stack, what changes do i need to bring about in the stack? Will it work if i configure any other GPIO pin as USB_ID pin or should i?

please help !

Thanks 
DIPIN

Labels (1)
0 Kudos
1 Reply

304 Views
Dipin
Contributor II

Hi All,

 

No comments from the Experts !?

 

0 Kudos