MCF51JM , XTAL Oscillator not running

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51JM , XTAL Oscillator not running

2,046 Views
Bloodhound
Contributor I

Hi All,

 

I'd been working with a prototype PCB using a MCF51JM, everything was progressing fine, then it just seemed to stop working, BDM cannot connect.

This is what I've found.

There is no oscillation on the XTAL/EXTAL pins (It's has an 8MHz crystal).

Reset line is pulsing every 40uS.

 

So far I've swapped in a new CPU, swapped 5V regs (it has a reset line) and the crystal, but this thing refuses to work now. Before it just quit it had been working ok and I was exectuing code on the MCU, so I know my circuit design is ok to at least make the thing functional.

 

So what might stop this CPU from running?

 

Thanks,

Ross

Labels (1)
0 Kudos
Reply
2 Replies

1,473 Views
Wanderer
Contributor II

I have a similar issue, but the reset line has a sawtooth from 2.6V to 3.3V.  What did you find was the issue with your board?


Thanks, gj

0 Kudos
Reply

1,473 Views
TomE
Specialist II

Search this forum for "KCF51JM", "crystal", "oscillator" and"MCGSC_OSCINIT".

 

This might be a starting point:

 

https://community.freescale.com/message/102052#102052

 

Tom

 

0 Kudos
Reply