I need to repair/chance processor of a lot of cards the: originally mounted(no avaliable): MC68332ACEH25 can be remplaced? by an option 1(more avaliable):MC68332GCEH25 or the option2: MC68332GCEH20 of option3:(almost not avaliable):MC68332ACEH20. i appretiate help thanks.
Hi Christian,
Out of curiosity I quickly checked the availablilty of your original part and found that DigiKey have 378 of them in stock.
Cheers, Shaun
i buy it just there in digikey but it was very very very hard to reach UPS to my place and the taxes payments another trouble, two month in total to get 3 processors form digikey, i prefer mouser just 5 days, but here only have the numparts i mencioned.
Element14 have the 20MHz part, X-ON (x-on.com.au) have the original part also, if that helps at all.
From memory, the 'A' or 'G' options refer to the microcode ROM version in the TPU, the 'A' being for automotive and the 'G' being for motion control. If your application uses the TPU then they cannot be interchanged but they probably can if the TPU is not used.
The '25' is the rated speed of the part in Mhz. If your boards are clocked at 20MHz or less then it should be okay to use the '20' part, otherwise results and reliablity will be unpredictable. Seeing that they originally used the 25MHz part, your boards are probably clocked at 25MHz.
Good luck.
Shaun
thank you so much