colilo>g 2000 Linux version 2.6.10 (pierrick@localhost) (gcc version 4.1.1 (CodeSourcery Sou ery G++ 4.1-30)) #18 Mon Feb 18 18:17:30 CET 2008 starting up linux rev 0.2: startmem 0xc029c000, size 61MB Built 1 zonelists Kernel command line: root=/dev/ram PID hash table entries: 512 (order: 9, 8192 bytes) RTC driver is not initialized yet, returning 1970. Console: colour dummy device 80x25 Dentry cache hash table entries: 16384 (order: 3, 65536 bytes) Inode-cache hash table entries: 8192 (order: 2, 32768 bytes) Memory: 62352k/65536k available (1976k kernel code, 1016k data, 96k init) Mount-cache hash table entries: 1024 (order: 0, 8192 bytes) NET: Registered protocol family 16 Linux/m68k PCI BIOS32 revision 0.05 ColdFire PCI Host Bridge (Rev. 0) detected PCI: Probing PCI hardware ColdFire internal SEC driver version 0.11 MCF547x/8x SEC device driver installed SCSI subsystem initialized NET: Registered protocol family 23 Initialize Multi-channel DMA API Alpha v0.3 (2004-04-26) JFFS2 version 2.2. (C) 2001-2003 Red Hat, Inc. Initializing Cryptographic API rtc: RV5C387 RTC driver successfully loaded ColdFire watchdog driver is loaded. MCF547x/8x DSPI device driver installed Coldfire DSPI driver is loaded ColdFire internal UART serial driver version 1.00 ttyS0 at 0xe0008600 (irq = 99) is a builtin ColdFire UART ttyS1 at 0xe0008700 (irq = 98) is a builtin ColdFire UART ttyS2 at 0xe0008800 (irq = 97) is a builtin ColdFire UART ttyS3 at 0xe0008900 (irq = 96) is a builtin ColdFire UART io scheduler noop registered io scheduler anticipatory registered io scheduler deadline registered io scheduler cfq registered RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize loop: loaded (max 8 devices) ColdFire internal FEC driver version 0.11 elevator: using anticipatory as default io scheduler Unlock all sector for Intel on Fire Engine... physmap flash device: 1000000 at f0000000 phys_mapped_flash: Found 1 x16 devices at 0x0 in 16-bit bank Intel/Sharp Extended Query Table at 0x0031 Using buffer write method cfi_cmdset_0001: Erase suspend on write enabled RedBoot partition parsing not available Using physmap partition definition Creating 2 MTD partitions on "phys_mapped_flash": 0x00000000-0x00040000 : "Colilo (256K)" 0x00040000-0x00200000 : "user (other Flash memory) 2Mb-256K" mice: PS/2 mouse device common for all mice i2c /dev entries driver i2c-algo-mcf.o: I2C ColdFire algorithm module is loaded. NET: Registered protocol family 2 IP: routing cache hash table of 1024 buckets, 8Kbytes TCP: Hash tables configured (established 8192 bind 16384) Initializing IPsec netlink socket NET: Registered protocol family 1 NET: Registered protocol family 17 NET: Registered protocol family 15 IrCOMM protocol (Dag Brattli) Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)