This is really an annoying message and it dumps a bunch of garbage as the system is booting up. Caused me a lot of confusion in getting my flash file system set up and working. My command line arguments first set up the "physmap-flash.0" then something else tries again. I also seem to have redundant physmap-flash entries in the /sys file system.
I do have flash working but this message will not go away and I've not been able to find it's source. Any help or suggestions would be MUCH APPRECIATED.
Thanks,
解決済! 解決策の投稿を見る。
Are you using the EVB board and bsp or a custom boar? Have you changed the kernel configuration? Check to make sure you arent enabling both compat physmap support and explicit physmap support.
If you cannot see what that you should do a service request and include the kernel config file and console messages showing uboot coming up on the board and the boot messages from the kernel.
- Coray