Linux 2.6.10 on MCF5485evb: Trouble configuring flexbus (or something...)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux 2.6.10 on MCF5485evb: Trouble configuring flexbus (or something...)

1,655 次查看
jkimble
Contributor III

I'm working with a custom board based on the MCF5485EBV board. I have several periferals attached to the Flexbus including flash, some general purpose latched i/o for leds and device resets, and the LCD display.

An issue that has raised it's ugly head is that when I can work the LCD display with graphics with no problem. I can work my leds (just board is alive indicators) with no problems. But when I work with them together the system crashes (locks up). I've checked my application and what I'm doing is so trivial (using /dev/mem and mmap to allocate memory and then setting the appropriate bit for an LED) that I'm 99% sure the problem must be with the mask I'm setting up when I initialize the Flexbus.

Any thought or ideas greatly appreciated. If I can't work out what's causing this my project is in serious jeopardy....

My flexbus configuration is as follows:

        // Code Flash (2x32MB Flash)
        MCF_FBCS_CSAR0 = FLASHBASE;
        MCF_FBCS_CSMR0 = 0x03ff0001;
        MCF_FBCS_CSCR0 = 0x00002500;            // 0x00004900

        // Init Chip selects 1, 2, 3, 4, 5
        MCF_FBCS_CSAR1 = CS1BASE;
        MCF_FBCS_CSMR1 = 0x000f0001;
        MCF_FBCS_CSCR1 = 0x00000000;

        // LEDs and Device Resets
        MCF_FBCS_CSAR2 = CS2BASE;
        MCF_FBCS_CSMR2 = 0x000f0001;
        MCF_FBCS_CSCR2 = 0x00000580;

        MCF_FBCS_CSAR3 = CS3BASE;
        MCF_FBCS_CSMR3 = 0x000f0001;
        MCF_FBCS_CSCR3 = 0x00000000;

        // LCD Display
        MCF_FBCS_CSAR4 = CS4BASE;
        MCF_FBCS_CSMR4 = 0x01ff0001;
        MCF_FBCS_CSCR4 = 0x00000080;

        MCF_FBCS_CSAR5 = CS5BASE;
        MCF_FBCS_CSMR5 = 0x000f0101;
        MCF_FBCS_CSCR5 = 0x00000580;



标签 (1)
0 项奖励
回复
1 回复

936 次查看
jkimble
Contributor III

Sorry, should have shown the configuration as:

// Code Flash (2x32MB Flash)
        MCF_FBCS_CSAR0 = 0xF0000000;
        MCF_FBCS_CSMR0 = 0x03ff0001;
        MCF_FBCS_CSCR0 = 0x00002500;         

        // Init Chip selects 1, 2, 3, 4, 5
        MCF_FBCS_CSAR1 = 0x41000000;
        MCF_FBCS_CSMR1 = 0x000f0001;
        MCF_FBCS_CSCR1 = 0x00000000;

        // LEDs and Device Resets
        MCF_FBCS_CSAR2 = 0x42000000;
        MCF_FBCS_CSMR2 = 0x000f0001;
        MCF_FBCS_CSCR2 = 0x00000580;

        MCF_FBCS_CSAR3 = 43000000;
        MCF_FBCS_CSMR3 = 0x000f0001;
        MCF_FBCS_CSCR3 = 0x00000000;

        // LCD Display
        MCF_FBCS_CSAR4 = 44000000;
        MCF_FBCS_CSMR4 = 0x01ff0001;
        MCF_FBCS_CSCR4 = 0x00000080;

        MCF_FBCS_CSAR5 = 45000000;
        MCF_FBCS_CSMR5 = 0x000f0101;
        MCF_FBCS_CSCR5 = 0x00000580;

0 项奖励
回复