LTIB build problem at package pkgconfig for Freescale M54418

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB build problem at package pkgconfig for Freescale M54418

965件の閲覧回数
francois_boucha
Contributor III

Hi,

Ltib build is failing at package pkgconfig,

 

MESSAGE:

(...)

checking for a BSD-compatible install... /usr/bin/install -c

checking for extra flags to get ANSI library prototypes... configure: error: cannot run test program while cross compiling

See `config.log' for more details.

configure: error: /bin/bash './configure' failed for glib-1.2.8

error: Bad exit status from /home/fbouchard/ltib/ltib-modelo-20100709/tmp/rpm-tmp.91454 (%build)

 

 

RPM build errors:

    Bad exit status from /home/fbouchard/ltib/ltib-modelo-20100709/tmp/rpm-tmp.91454 (%build)

Build time for pkgconfig: 14 seconds

 

Failed building pkgconfig

 

 

f_buildrpms() returned an error, exiting

traceback:

main:560

 

 

Started: Fri Mar 22 16:58:16 2013

Ended:   Fri Mar 22 16:59:16 2013

Elapsed: 60 seconds

 

These packages failed to build:

pkgconfig

 

Build Failed

 

Exiting on error or interrupt

 


 

Now in a post I saw if I understand correctly, this package isn't meant for the Coldfire processors

--> http://comments.gmane.org/gmane.comp.package-management.pkg-config/342

Hi,

 

Enrico> The bundled glib-1.2.10 is not crosscompile'able.

 

Enrico> Look at glib-1.2.10/configure.ac: once you use AC_TRY_RUN, your

Enrico> package cannot crosscompile. A very common standard error in

Enrico> autoconf-based packages ...

 

But if you build with an external libglib (--with-installed-glib) it

builds without problems.

 

- tried in pkconfig.spec (made backup of the original)

 

 

I tried the trick above but it didn't work.

 

 

Any hints on how to compile pkgconfig?

 

Francois

 


ラベル(1)
0 件の賞賛
1 返信

455件の閲覧回数
francois_boucha
Contributor III

I found the error.

Somehow the temporary script is not going into the right directory.

See in bold:

Processing: pkgconfig

=======================

(.......)

Building for target m68k

Executing(%build): /bin/sh -e /home/fbouchard/ltib/ltib-modelo-20100709/tmp/rpm-tmp.12682

+ umask 022

+ cd /home/fbouchard/ltib/ltib-modelo-20100709/rpm/BUILD

+ ./configure --prefix=/usr --host=m68k-linux --with-internal-glib

/home/fbouchard/ltib/ltib-modelo-20100709/tmp/rpm-tmp.12682: 1: ./configure: not found

error: Bad exit status from /home/fbouchard/ltib/ltib-modelo-20100709/tmp/rpm-tmp.12682 (%build)

Instead it should go to here : /home/fbouchard/ltib/ltib-modelo-20100709/rpm/BUILD/pkg-config-0.28, but I don't know what to modify.  Would it be the specfile?

0 件の賞賛