Is C_4i_CF_FPU_Runtime.a and C_4i_CF_FPU_MSL.a required?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is C_4i_CF_FPU_Runtime.a and C_4i_CF_FPU_MSL.a required?

1,224件の閲覧回数
christoph_bayer
Contributor I
Hello,
we use the CF 5484 Processor.
We use the C_4i_CF_FPU_MSL.a, but not the C_4i_CF_FPU_Runtime.a.
Does we need the Runtime or is it included in the MSL?
Does we need it for Debugging?
 
Thanks
cba
ラベル(1)
0 件の賞賛
返信
1 返信

686件の閲覧回数
CrasyCat
Specialist III
Hello
 
C_4i_CF_FPU_Runtime.a contains run time code for Coldfire CPU.
This runtime code is not included in the MSL library, so you need to add both library files to your project.
 
Run time library includes startup code plus some additional functions for long and long long arithmetic, setjump and others.
 
This library is already required at link time.
Note that as the linker is performing dead stripping, if the library is not needed, there will be no superfluous code linked to the application. So my recommendation is to always add both libraries to a project.
 
CrasyCat
0 件の賞賛
返信