Interrupt 5275EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interrupt 5275EVB

3,341 次查看
bizio
Contributor I
Hi all,
I'm working with 5275EVB.I have a problem with the management of the interrupts generated by the UARTs. The source code used to inizialize the UARTs is the following:

MCF_UART_UCR1 = MCF_UART_UCR_RESET_TX;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_TX;

MCF_UART_UCR1 = MCF_UART_UCR_RESET_RX;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_RX;

MCF_UART_UCR1 = MCF_UART_UCR_RESET_MR;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_MR;

MCF_UART_UMR1 = (0
| MCF_UART_UMR_PM_NONE
| MCF_UART_UMR_RXIRQ
| MCF_UART_UMR_BC_8 );
MCF_UART_UMR2 = (0
| MCF_UART_UMR_PM_NONE
| MCF_UART_UMR_RXIRQ
| MCF_UART_UMR_BC_8);

MCF_UART_UMR1 = (0
| MCF_UART_UMR_CM_NORMAL
| MCF_UART_UMR_SB_STOP_BITS_1);
MCF_UART_UMR2 = (0
| MCF_UART_UMR_CM_NORMAL
| MCF_UART_UMR_SB_STOP_BITS_1);

MCF_UART_UCSR1 = (0
| MCF_UART_UCSR_RCS_SYS_CLK
| MCF_UART_UCSR_TCS_SYS_CLK);
MCF_UART_UCSR2 = (0
| MCF_UART_UCSR_RCS_SYS_CLK
| MCF_UART_UCSR_TCS_SYS_CLK);


MCF_UART_UIMR1 = MCF_UART_UIMR_RXRDY_FU;

MCF_UART_UISR1 = MCF_UART_UISR_RXRDY_FU;

MCF_UART_UIMR2 = MCF_UART_UISR_RXRDY_FU;

MCF_UART_UISR2 = MCF_UART_UISR_RXRDY_FU;


ubgs = (uint16)((SYSTEM_CLOCK*1000000)/(9600 * 32));

MCF_UART_UBG1(1) = (uint8)((ubgs & 0xFF00) >> 8);
MCF_UART_UBG2(1) = (uint8)(ubgs & 0x00FF);

ubgs = (uint16)((SYSTEM_CLOCK*1000000)/(4800 * 32));

MCF_UART_UBG1(2) = (uint8)((ubgs & 0xFF00) >> 8);
MCF_UART_UBG2(2) = (uint8)(ubgs & 0x00FF);


MCF_UART_UCR1 = (0
| MCF_UART_UCR_TX_ENABLED
| MCF_UART_UCR_RX_ENABLED);
MCF_UART_UCR2 = (0
| MCF_UART_UCR_TX_ENABLED
| MCF_UART_UCR_RX_ENABLED);

At the beginning it runs correctly, but after some interrupts received the CodeWarrior goes on error.
The error is "Address Error".
Someone can help me to resolve this error?
Thank you in advance for your help.

Message Edited by bizio on 2006-06-19 03:17 AM

标签 (1)
0 项奖励
回复
2 回复数

989 次查看
mvincent
Contributor I
Something to check: make sure you have programmed the interrupt controller's ICRs with unique interrupt level/priority. Also, make sure all the code and structures involved in the service routines are reentrant or in critical sections.
0 项奖励
回复

989 次查看
fire
Contributor I

hai,

I faced the same problem and i strugled for days.

The problem is with nesting of interrupts.If u are disabling the global interrupt any where, do it in the correct way.

let me know whether you are disabling the interrupts any where.Give me the correct details.

ALL THE BEST.

0 项奖励
回复