I want to convert BIN file to abs or S19 file. help me please.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to convert BIN file to abs or S19 file. help me please.

6,346 Views
vinoddevrari
Contributor II

hello i have a coldfire processor. I want to copy a program on this processor with the help of CYCLONE FX . This processor is only read S19 or ABS file but i have BIN. file. How can i do it ,help me please.

thanks 

vinod devrari

Devrariv@gmail.com

2 Replies

4,811 Views
miduo
NXP Employee
NXP Employee

Hi,

 You may would like try with this tool: www.s-record.com 

4,811 Views
TomE
Specialist II

What toolchain are you using? What compiler and so on?

Or are you trying to copy the code from one chip to another one without using a toolchain?

Toolchains come with programs to convert one binary format to another. For instance, the gcc tools have "objcopy" and on my computer there's "m68k-elf-objcopy" which is the one for the Coldfire toolchain.

You're using a PE Micro product, so you should be looking for answers on PE Micro's Forum. Here's someone asking how to convert ABS to S19 files, an PE Micro answers with a link to a program to do just that.

http://www.pemicro.com/forums/forum.cfm?forum_topic_id=5147

Tom