How to debug on my K64F on IAR using windows in a virtual machine?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to debug on my K64F on IAR using windows in a virtual machine?

818件の閲覧回数
bayrammidassi
Contributor I

Hallo,

i have a problem to debug my Program which is developed on IAR using CMSIS/DAP on windows.

I am using Linux mate as the main OS and Windows in the virtual machine.

The problem is that windows does't detect the USB interface of my card K64F.

I added the card like a shared disc to my virtual machine but it does't work.

 

Any help?

thanks in advance

ラベル(1)
0 件の賞賛
返信
1 返信

731件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Have you tried the Vmware? From what I know the best way to run a virtual machine with real hardware is to use VMware and run a virtual XP session... it should works good with all sorts of USB drivers that seem to have trouble on win 7 and other virtual machines.. Be warned that VMware must take over exclusive use of the USB ports while running..

0 件の賞賛
返信