Has anyone designed with MCF5327?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Has anyone designed with MCF5327?

2,006 次查看
Blondie09
Contributor I
I have had problems communicating with the MCF5327. It looks like on my board that the reset pin stays low all the time and never comes out of reset. Does anyone have any ideas?? I need help ASAP!!!
 
Also, I can not to put the program in flash because it says me that "Cannot connect with the BDM" but it is connected.
标签 (1)
0 项奖励
回复
3 回复数

1,105 次查看
JWW
Contributor V
Can you share a bit more information for the community to help?  Many of us have done design work on the 532x family. 
 
What basic debug steps have you already done?
 
-JWW
 
0 项奖励
回复

1,105 次查看
rtribaudino
Contributor I
Sorry , i did a mistake.
OK your problem is the release of datasheet that you have used.
if you design your application with revision 3 there are 19 pins of map BGA 196 pin wrong.
You need use Rev4.
 
Bye
Riccardo
0 项奖励
回复

1,105 次查看
rtribaudino
Contributor I
Yes I did,
can i help you?
 
Riccardo
0 项奖励
回复