Experience with GCC for Coldfire and 9s12......

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Experience with GCC for Coldfire and 9s12......

3,546 Views
nikhilthiruveng
Contributor I

Hi Guys,

Has anyone got experience in working with GCC for Coldfire and 9s12 processors.

Recommendations on what GCC to use????

Thanks in advance

N

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

2,297 Views
thm59
Contributor II

Hello,

I successfully use GCC/GDB from Codesourcery on coldfire V1 MCUs, with the Eclipse IDE on Win 7. I use the free “lite” version with a (very) low-cost USBDM debugger. I use the USBDM because the lite version of codesourcery  doesn’t include a flasher, and PGO (the great autor of USBDM) provides a free standalone flasher along with an interface dll for GDB

See :

http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/code_sourcery_page.html

or

http://myfreescalewebpage.free.fr/tutorials/tutorial_codesourcery/tutorial_codesourcery.htm

It should normally be possible to do the same with V2-V4 coldfire mcus, but I haven’t try.

See also the "OSBDM" forum for more information.

As far as I know, GCC for MC9S12 is no longer supported

Thierry


2,297 Views
JimDon
Senior Contributor III

Sadly, the Firebird32 in no longer in production.

I have a few left, but you can no longer buy them.

Like the page that is to linked says , I did write a fairly complete Wiring Framework for V1, which one of my customers is using.

If any one is interested, it is open sourced.

http://www.firebird32.com/

0 Kudos
Reply

2,297 Views
TomE
Specialist II

We use the CodeSourcery package.

CodeSourcery got bout out by Mentor Graphics. They still seem to have a Free/Lite version available:

http://www.mentor.com/embedded-software/sourcery-tools/sourcery-codebench/editions/lite-edition/

The very least you need is a working cross-compiler and cross-linker with C libraries built for the target. The usual tools like nm, gdb, objdump and so on are also useful. That's all we took from the CodeSourcery package, together with a version of "make" that runs under windows. We managed to get the gcc to talk to a USB pod and debug it that way, from the gdb command line.

If you already have a complete working code base (including operation system or event-loop and device drivers) then that's all you need.

If you want a fully featured "integrated development environment" that works like Visual Studio does, then you might be able to use Eclipse, but I've never had any luck with it.

Tom

2,297 Views
ReeL
Contributor I

Hi N,

I use the RTEMS precompiled m68k tools under CentOS to build for MCF52235, MCF52259 and MCF5235.  I have not tried building my own GCC binaries or using them from anyone else.  I have no experience with the 9S12 processors sorry.

Leon

0 Kudos
Reply