Does the MC68EC000AA10 have an MMU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the MC68EC000AA10 have an MMU?

3,205 次查看
carterson2
Contributor I
I wanna run linux on the cheapest processor.
Not uClinux, rather FULL-linux.
 
Soo, I am researching the cheapest processor (WITH an MMU).
 
thanks guys!!!
标签 (1)
0 项奖励
回复
5 回复数

1,293 次查看
carronjack
Contributor I
Hi,
   No it doesn't,but why do you need one?

Regards Ian


0 项奖励
回复

1,293 次查看
w_wegner
Contributor III
Hi,

he wrote why he needs one: he wants to run linux, not uClinux.

And, I have to admit that meanwhile I can understand that. I am trying to get my uClinux system running for several weeks now, and there are definitely many problems and disadvantages...
(Seemingly especially in m68knommu, although I do not understand why this is the case as that was the architecture originally bringing uClinux to life. :smileysad: )

Regards,
Wolfgang
0 项奖励
回复

1,293 次查看
carterson2
Contributor I
I am writing an article on the cost of MMU vs nonMMU and I need to know the cheapest MMU processor.
 
Do you know which is motorola's cheapest MMU processor, or might it be Intel or some other?
 
thanks for any leads.
jim
0 项奖励
回复

1,293 次查看
Nouchi
Senior Contributor II
Hi,

If you want to stay in the 68K world, you can use originals MC68030, 040 and 060, but I don't think that are the cheapest parts.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MC68030&nodeId=0162468rH3YTLC61654622...

The MCF54450CVM180 seems to be the cheapest parts with MMU in the 68K architecture
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5445X&nodeId=0162468rH3YTLC00M9342...

Now you can find the MC9328MX21VM with arm9 architecture
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX21&nodeId=0162468rH311432973ZrDR&...


EMMANUEL


0 项奖励
回复

1,293 次查看
carronjack
Contributor I
Hi,
  68030 used in most older CISCO routers, pretty cheap on Ebay,at least 1 68040 for sale, also on Ebay
 if you want to go 68K route.

Best Regards
Ian

P.S. Sorry about my previous post,Looked like I was Shouting ( Wrong Font + Size )
0 项奖励
回复