Colfire 1, this uses a lot of current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Colfire 1, this uses a lot of current

934件の閲覧回数
Gabriel_Medelli
Contributor I

Good night, someone can tell me if the ports must be configured as either inputs or outputs, and that way, to avoid the high current consumption of the system, since apparently the current absorbed by colfire unused ports.

thanks

Regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

819件の閲覧回数
TomE
Specialist II

What current are you measuring? What do you expect (and what section of what data sheet are you reading)?

 

What MODES do you have the CPU running in, what clock speed and so on?

 

Can you separately measure the CPU current and that being used by the rest of your board?

 

You should be on the Coldfire forum for these questions.

 

Tom

 

0 件の賞賛
返信

819件の閲覧回数
rocco
Senior Contributor II

Hi Gabriel,

 

Welcome back to the forum.

 

I don't have direct experience with Coldfire-1, but in general, if an input pin is left to float between the rails, then they can draw a lot of current. If an input is not driven, then it should have a pull-up or pull-down resistor to bring it to one of the rails. Most newer Freescale MCUs have built in pull-ups, but they are typically enabled under software control, and might default to disabled. The safest thing to do with unused I/O is to program them as outputs.

0 件の賞賛
返信