Cannot transfer uImage through tftp under linux on MCF5485EVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot transfer uImage through tftp under linux on MCF5485EVM

1,872 次查看
chuang39
Contributor I

Hi,

 

I'm trying to transfer uImage to MCF5485 board under linux. But when I enter "tftp 02000000 uImage", the responce is " T T T T".

 

I set the IP of eth1 of host pc as 192.168.1.2.

The board configuration is as below:

IPADDR=192.168.1.110

NETMASK=255.255.255.0

SERVERIP=192.168.1.2

 

I was able to use tftp under windows. So i think the board configuration was fine. The only thing i did under windows was to fix the IP address of eth1 adapter. I did the same thing in linux, but I could not use tftp under linux. I used "iptable -F" to turn off the firewall in linux. The tftp was running. I was able to ping host from target board under both windows and linux.

 

Can anybody give me some advice? Thanks very much!!

 

Chuan

标签 (1)
0 项奖励
回复
2 回复数

1,043 次查看
bbjh1
Contributor I

Hi chuang39

 

I know it has been a long time since you posted this thread but I was wondering how did you fix your problem? Thank you.

 

bbjh1

0 项奖励
回复

1,043 次查看
jkmahan
Contributor III

Can you ping the server (192.168.1.2) from your board?

 

Is the TFTP running on your server?

0 项奖励
回复