Can we use SDA and SCL pins for UART in MCF5206E? If yes, how?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use SDA and SCL pins for UART in MCF5206E? If yes, how?

2,822 Views
vidyahegde
Contributor I

How can we use SDA and SCL pins as RX and TX pins of UART in MCF5206E

2 Replies

1,763 Views
miduo
NXP Employee
NXP Employee

Hi,

Yes, as Tom metioned, MCF5206 is quite old and all pins do not have the multi-fucntion as the later ColdFire parts are. So you can not use the SDA/SCL as UART RX & TX.

1,763 Views
TomE
Specialist II

You can't.

This is a 22 year old design. All the pin functions are fixed. Being able to reassign pins to different function modules (and use them as GPIOs) was only added in later ColdFire models.

You could always use an external chip which provides a UART function and has an I2C (aka M-BUS) interface.. Which is just about any modern single-chip microprocessor programmed to do that.

Or, already set up to do exactly this (thank you Google), the NXP SC16IS740:

https://www.sparkfun.com/products/retired/9981

https://www.nxp.com/products/analog/signal-chain/bridges/single-uart-with-i2c-bus-spi-interface-64-b...

Tom