Can someone explain Interrupt Levels and Priorities

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can someone explain Interrupt Levels and Priorities

4,018 次查看
WOLF
Contributor I
I am using the Eport interrupts on a design, and I dont fully understand Priorities and Levels.  I see in the Reference manual that they have a preset/Unchangeable Priority.  but what about level?  how does it all work together.   how does level and priority relate to interrupt servicing?
 
 
Thanks in advance,
 
标签 (1)
0 项奖励
回复
6 回复数

2,079 次查看
admin
Specialist II
This is easy.
Imagine that the CPU is servicing an interrupt with level N. Then an interrupt request with level M activates. If M>N then the CPU will start processing the new interrupt, otherwise it will finish processing the first interrupt before starting to process the next. That's how levels work. Level 7 is special, the above doesn't apply to it.
Now imagine that there are several pending interrupt requests with the same level. That's where priorities come in. The one with the highest priority will be serviced first, others will wait. Then if a new interrupt request activates with the same level and a higher priority, it will still wait. Unlike levels, priorities do not preempt each other.
EPORT is special: it has a 'fixed midpoint priority' between 3 and 4. You can think of it as having priority 3.5. The interrupt level is still configurable, though.
0 项奖励
回复

2,079 次查看
admin
Specialist II
Thank you, Georg, for correcting me. I wasn't too careful reading the manual. Of course, EPORT's interrupt level is not configurable. Looking into the manual for my MCU (MCF52233), I cannot see which level is used by EPORT.
0 项奖励
回复

2,079 次查看
taigbr
Contributor I
Hi Scifi,

take a look at:
http://www.freescale.com/files/32bit/doc/ref_manual/MCF5275RMAD.pdf?fpsp=1
I don't know if this scheme works for all coldfire mcus.
Regards, Georg


0 项奖励
回复

2,079 次查看
WOLF
Contributor I
Thank you both, this has help me to understand them.. 
 
0 项奖励
回复

2,079 次查看
taigbr
Contributor I
Hi Wolf,
there is a nice picture in the ref manual addendum for the 5275 showing the
priority levels. But it states that the eport ints are of mid priority, but all with
a different int level. Irq5 is level 5 and mid priority, Irq1 is level 1 and mid priority.
They are not all allocated at level 3.
Regards, Georg
0 项奖励
回复

2,079 次查看
JimDon
Senior Contributor III
Simply stated, a level has a priority, and then with in that level there is a "sub-priority" called the "priority".

Levels can be locked out, but once a level is enabled all devices on that level will be serviced based on the priority within the level.

You should say which chip, as different ones have different ways you can address this.
Some chips you can set both the level and priority others no.



0 项奖励
回复