COLD FIRE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

COLD FIRE

4,692 次查看
rao
Contributor I
Hai all,
 Can anybody  sedn an example code which explains the usage of general purpose timer module in mcf5282.
Please include initialization of various memories like SDRAM  ,IPSBAR etc..
  Thanks in advonce.
标签 (1)
0 项奖励
回复
4 回复数

1,538 次查看
mpeters
Contributor I
Rao,

Sample code that shows all of the initialization of the processor, memories, etc., can be downloaded from the MCF5282 product summary page. It is located in the "Software" section, and the link is entitled "MCF5282SC". Here is the link to the MCF5282 product summary page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5282&nodeId=0162468rH3YTLC00M95448

We don't have any code specifically for the GPT on the MCF5282, however attached is some code that was written for the GPT on the MCF5213. The MCF5282 and MCF5213 use the same GPT module, so this is a good reference and the code should be helpful to you.

Regards,
mpeters

Message Edited by mpeters on 04-11-2006 10:55 AM

0 项奖励
回复

1,538 次查看
rwehrli
Contributor I
mpeters,

Do you also happen to have PIT timer sample code? I've been able to configure the timer, but haven't been able to get it to produce an interrupt on the M5211DEMO board using CW 6.4.

In my mcf5xxx_vectors.s I have at the top:


.extern IRQ_PIT0

...nothing else changed until...

vector055: .long IRQ_PIT0

In main.c I have:

void IRQ_PIT0( void )
{
printf( "IRQ_PIT0\r\n" );
}

And, interestingly, if I don't make a call to it in main, IRQ_PIT0 is never linked as a defined symbol, as shown in the produced map file.

So, I put a call to it at the top of main, found it my linker map, but still no interrupt.

MCF_PIT0_PCSR = 0x023B;
MCF_PIT0_PMR = 0x0040;

...is my current PIT0 configuration. Perhaps I've got things improperly configured?

Is there some other method of configuring interrupt handlers that I haven't yet figured out? I've only had about 3 hours with this board.


Take Care.

Rob!
0 项奖励
回复

1,538 次查看
mccPaul
Contributor I
Hi
 
 
This is specifically aimed at the mcf5282, but the timers are very similar, if not identical between the Coldfire parts, just check the manual if you aren't using the 5282.
 
Paul.
0 项奖励
回复

1,538 次查看
rao
Contributor I
Thank you Mr Mpeters.
0 项奖励
回复