Hello, all
My board run under BDM and Backup Watchdog Timer init with Processor Expert bean. But, when I break debug (stop Run) Backup Watchdog Timer NOT reset MCU and I read WCNTR = 0000, even when my programm write 0x5555 0xAAAA to WSR. My configuration:
CLKMOD[01] = 01 (CLKMOD0 pin have pullup resistor, XTAL pin NOT have pullUP resistor)
BWCR (CLOCK MODULE) = 0x00 - 32 MHz from bus
WCR = 0x0003
WMR = 0xFFFF - 8388,48 ms timeout
Init function:
void Wtm1_Init(void)
{
/* WMR: WM=0xFFFF */
setReg16(WMR, 0xFFFFU);
/* WCR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,STOP=0,WAIT=0,DOZE=0,??=1,EN=1 */
setReg16(WCR, 0x03U);
}
Can I check software reset in the debug mode?
P.S. I use CW version 5.9.0 build 5293
Thank for answer
Hi Sergey,
The ColdFire BWT is good for production application but not good for debugging mode. The BWT clock continues clocking even when you hit a breakpoint (which stops the core but it not the same as implementing a STOP instruction).
You could use the internal (slower) clock rather than the 32MHz to increase the timeout period.
Regards,
David