Availability of M53015EVB Schematics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Availability of M53015EVB Schematics

Jump to solution
2,022 Views
ReeL
Contributor I

Does anyone know where I might be able to get a copy of the schematics for the M53015EVB?  I would like to check the details of its features before committing to buy one.

Labels (1)
0 Kudos
Reply
1 Solution
1,200 Views
Dec
Contributor III
0 Kudos
Reply
5 Replies
1,200 Views
admin
Specialist II

Hi,

I would like also to check some details concerning dual phy layers. Could you share a copy of the schematics of the M53015EVB if you keep it? I'll be appreciated!

0 Kudos
Reply
1,200 Views
ReeL
Contributor I

Hi,

I still have a copy but can't upload it with this response sorry.  If you go to the downloads page for the M53015EVB you will find a download called "M53015EVB - Printed Circuit Board bill of materials and design files: Available files and documentation for printed circuit board manufacturing".  This contains a PDF of the schematics - and other things.

0 Kudos
Reply
1,201 Views
Dec
Contributor III

This one ?

 

0 Kudos
Reply
1,200 Views
ReeL
Contributor I

Thanks Dec,

 

Yes it looks like the one I was after.  Thank-you :smileyhappy:

 

I saw your post of https://community.freescale.com/message/66796#66796 We are looking at using the LQFP for a design too so I have added a question for you there.

 

Thanks again

0 Kudos
Reply
1,200 Views
J2MEJediMaster
Specialist I

The closest thing I have found is the M53015EVBUM User Manual, which has a block diagram of the board. The manual does not have schematics, however.

 

---Tom

 

0 Kudos
Reply