Auto Negotiates - MCF52233 not working on a 1Gbit switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Auto Negotiates - MCF52233 not working on a 1Gbit switch

1,727件の閲覧回数
PeterKirketerp
Contributor I

Hi

 

The old version of the MCF52233 chip had a problem with the Auto Negotiates. I have now received new samples of the chip 1/3-2007. On an old switch 10/100Mbit the Auto Negotiates is working fine, but when I am using a 1Gbit switch I still have problem!

 

Any help?

 

Peter Kirketerp

Develco A/S

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

972件の閲覧回数
Cremericon
Contributor I
Hi
 
Whats is the status on the auto negotiates?
 
Have just got some samples that has the issue with the auto negotiates.
Have the problem been solved?
If so from what production week must the chip be.
 
Regards
Steen
0 件の賞賛
返信

972件の閲覧回数
macl
Senior Contributor I
The new version with auto negotiation fixed is not available yet.  I suspect that the devices you have are working with the 10/100 switch because of device to device variations.  Some devices may actually work but some will not.  The 1Gbit switch is more stringent than the other switch, therefore the current version of the device is less likely to work.  The 1Gbit switch may be sending shorter link pulses and the device is not able to recognize them.  We are addressing this problem and expect the fixed version to be available later this year. 
0 件の賞賛
返信