Any higher processor supports HTTP authentication then MCF5223X series?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Any higher processor supports HTTP authentication then MCF5223X series?

919 次查看
TVNAIDU
Contributor III

Any higher processor supports HTTP authentication then MCF5223X series?. Like password auth, also change passwords, different user accounts like it comes in Embedded LINUX tiny web server. Looking in micro-controller like MCF5223x series only,

标签 (1)
0 项奖励
回复
1 回复

608 次查看
scifi
Senior Contributor I

I'm not sure I understood the question.

Anyway, I have implemented a web server with HTTP Digest Authentication on a MCF5223x. HTTP Basic Authentication would be even easier to implement. User accounts would be trivial to do as well. So yes, it is possible.

0 项奖励
回复