An MCF51 MCU I'd love to see

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An MCF51 MCU I'd love to see

794 Views
Bloodhound
Contributor I

I'd like to see a device in the MCF51JM series with CAN in a 32LQFP package, or even in the existing 44LQFP they offer (that doesn't currently have CAN, why?). Drop some of the other modules if needed, USB could go for Automotive use.

Currently CAN is only available in the 64LQFP or 80LQFP packages (eg MCF51JM32VLH), this is a PITA for the hobbyist (maybe Freescale don't care about this market segment). The pricing on the MCF51JM series is fantastic, however nearly all of Freescale's competitors offer small pin count devices with CAN (eg Atmel, Microchip). They also have similar pricing to the MCF51JM series, so it makes it tough to stay loyal to Freescale for anyone that needs CAN but doesn't want a 64 pin device to get it.

Labels (1)
0 Kudos
Reply
2 Replies

597 Views
Mickey
Contributor III

Hi, You can choose "MC9S08DZxxCLC", LQFP32package.

0 Kudos
Reply

597 Views
Bloodhound
Contributor I

Okay, but that isn't even a Coldfire device.

0 Kudos
Reply