An MCF51 MCU I'd love to see

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

An MCF51 MCU I'd love to see

1,427 次查看
Bloodhound
Contributor I

I'd like to see a device in the MCF51JM series with CAN in a 32LQFP package, or even in the existing 44LQFP they offer (that doesn't currently have CAN, why?). Drop some of the other modules if needed, USB could go for Automotive use.

Currently CAN is only available in the 64LQFP or 80LQFP packages (eg MCF51JM32VLH), this is a PITA for the hobbyist (maybe Freescale don't care about this market segment). The pricing on the MCF51JM series is fantastic, however nearly all of Freescale's competitors offer small pin count devices with CAN (eg Atmel, Microchip). They also have similar pricing to the MCF51JM series, so it makes it tough to stay loyal to Freescale for anyone that needs CAN but doesn't want a 64 pin device to get it.

标签 (1)
0 项奖励
回复
2 回复数

1,230 次查看
Mickey
Contributor III

Hi, You can choose "MC9S08DZxxCLC", LQFP32package.

0 项奖励
回复

1,230 次查看
Bloodhound
Contributor I

Okay, but that isn't even a Coldfire device.

0 项奖励
回复