AN3906 Ethernet to Serial Bridge - how to expand?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN3906 Ethernet to Serial Bridge - how to expand?

515 次查看
philbr
Contributor I

I am looking to expand your application note AN3906 (using MCF51CN Ethernet microcontroller family) to go from an ethernet interface to multiple serial ports. My idea would be to set up the FreeRTOS  for each serial port to be a thread with an ethernet thread receiving/sending ethernet packets and dispatching to/from various serial ports. This is an internal network not connected to the internet and implementing a custom message layer via TCP not UDP. Obviously I would need to handle flow control separate for each serial port but there are no hard real time requirements. Are there additional considerations under this approach?  I would like to handle up to 8 serial devices (maybe more?) as these are not real time devices (sensors like temperature monitoring, etc)

 

Thanks for any thoughts,

-Phil B

标签 (1)
0 项奖励
回复
0 回复数