68332 - What is available in source level debug ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

68332 - What is available in source level debug ?

941 次查看
Alex_J
Contributor I
I am looking for a source level debug environment for MC68332.
In the past few days my associate contacted Avocet and P&E. These two companies had debuggers in the past but are no longer supplying for 68 K processors.
I want to buy:
- the hardware interface to the 68332 Background Debugging Mode
- the driver or support software for source level debugging.
I have read freescale's application note AN1230/D, from which it seems not difficult to setup the debug mode, but I want something with source level.  That is, to set one or more break points from a window showing the source level file, single step at the source level, examine ram using variable names.
Please reply if you have any suggestions.

 

 

Message Edited by Alex_J on 2008-02-29 09:00 PM

 

Message was edited by: Alexander Hamburger

 

Message was edited by: Alexander Hamburger  I found these two companies give debug tools.  1. WindRiver.  Supplies a backround debug mode probe. Works great but does not insert breakpoints in flash memory. If your code is in RAM you are ok. If your code is in flash, you can still program flash, erase flash, reset the micro, start and stop the micro, copy memory to your pc, and several other useful things.  2. Lauterbach.  A full debugger.

标签 (1)
0 项奖励
回复
0 回复数