downloading Codewarrior 10.9 for Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

downloading Codewarrior 10.9 for Linux

跳至解决方案
2,565 次查看
d_li
Contributor III

I can't seem to find a codewarrior 10.9 install for linux. The file on the site seems to only have the toolchain and not eclipse. I have not been able to find one w/ eclipse, but the readme from the toolchain archive seems to indicate that it should be used with the eclipse based IDE

标签 (1)
0 项奖励
回复
1 解答
2,054 次查看
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,055 次查看
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

0 项奖励
回复
2,054 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi David,

The CodeWarrior for StarCore 3900 FP is the the only CodeWarrior Software that matches the version 10.9.0 and it can be downloaded from this link

CodeWarrior Dev Tools for StarCore 3900FP DSP|NXP

Regards,

0 项奖励
回复