Hello,
I am just playing around with the MCS8156EVM Board. While checking the different options for the project wizard it seems to me that the option 'trace and profile' (step 7/7) is only available if SmartDSP OS (step 4/7) is set to 'no'. Is this true ? any reasons ? any workarounds to use the trace and profile functionality and SmartDSP in the same project ?
Best Regards
Markus
已解决! 转到解答。
There is trace functionality for the MSC8156EVM with or without SmartDSPOS. What version and build number of the tools are you using? I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?
Regards,
Irene
There is trace functionality for the MSC8156EVM with or without SmartDSPOS. What version and build number of the tools are you using? I just verified on the latest toolset and I was able to set trace and profile for MSC8156EVM for SmartDSPOS and without SmartDSPOS?
Regards,
Irene
Hi Irene,
thanks for the hint. I just updated everything that is preset in the 'availabe software sites' dialog box and afterwards I can choose SmartDSP OS and trace functionality in one project.
Best Regards
Markus