SRIO ID MSC8156

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SRIO ID MSC8156

跳至解决方案
1,637 次查看
Kirill
Contributor I

Hello!

 

I could not find attribute to change SRIO ID from 16 bits to 8 bits,  what fucntion should I use or sructure?

 

Thank you!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,285 次查看
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,286 次查看
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

0 项奖励
回复