Codewarrior morpho.core errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior morpho.core errors

Jump to solution
3,986 Views
d_li
Contributor III

When using CW, I get errors such as

 

130524_130524.png2016-01-21 10_30_38-C_C++ - CodeWarrior Development Studio.png

130525_130525.png2016-01-21 10_31_46-Trace configuration load error for test_ftpe_b4860 - Core 0 - Debug.png

 

When I try to access the debug settings for a project. I have tried uninstalling and installing CW 10.9 again to no avail.

 

Followup: Not sure if this is relevant but I tried the following also in an attempt to fix this.

 

C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse>register_xpcom.bat

Registering...

ERROR:xpcom:Unhandled exception calling 'int8 loadModule(in nsISomething, out retval nsISomething);'

Traceback (most recent call last):

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\policy.py", line 277, in _CallMethod_

    return 0, func(*params)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\loader.py", line 92, in loadModule

    return self._getCOMModuleForLocation(aFile)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\loader.py", line 108, in _getCOMModuleForLocation

    py_mod = loader.load_module( module_name_in_sys, stuff )

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\ihooks.py", line 272, in load_module

    m = self.hooks.load_source(name, filename, file)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\ihooks.py", line 170, in load_source

    return imp.load_source(name, filename, file)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.sa_2.0.0.154851-201511241342\morpho\sa\SaHWTestSetup.py", line 2, in <module>

    import telnetlib

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\telnetlib.py", line 39, in <module>

    import socket

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\socket.py", line 47, in <module>

    import _socket

ImportError: DLL load failed: The specified procedure could not be found.

ERROR:xpcom:Unhandled exception calling 'int8 loadModule(in nsISomething, out retval nsISomething);'

Traceback (most recent call last):

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\policy.py", line 277, in _CallMethod_

    return 0, func(*params)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\loader.py", line 92, in loadModule

    return self._getCOMModuleForLocation(aFile)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\xpcom\server\loader.py", line 108, in _getCOMModuleForLocation

    py_mod = loader.load_module( module_name_in_sys, stuff )

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\ihooks.py", line 272, in load_module

    m = self.hooks.load_source(name, filename, file)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\ihooks.py", line 170, in load_source

    return imp.load_source(name, filename, file)

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.sa_2.0.0.154851-201511241342\morpho\sa\SaHWTestSetup.py", line 2, in <module>

    import telnetlib

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\telnetlib.py", line 39, in <module>

    import socket

  File "C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\socket.py", line 47, in <module>

    import _socket

ImportError: DLL load failed: The specified procedure could not be found.

Exception KeyError: KeyError(5652,) in <module 'threading' from 'C:\Freescale\CW_SC_3900FP_v10.9.0\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\python\lib\threading.pyo'> ignored

Labels (1)
0 Kudos
Reply
1 Solution
3,237 Views
Anonymous
Deactivated User

Hi David,

can you please remove the below plug-in from CW installation directory and  check if the behavior change!!

<installation dir>\eclipse\plugins\com.freescale.sa_2.0.0.154851-201511241343

BR

Marc

View solution in original post

0 Kudos
Reply
8 Replies
3,238 Views
alexandraarcali
NXP Employee
NXP Employee

Hi David,

These 2 errors you are seeing are actually SA (Software Analysis) component loading issues caused by SA being unable to retrieve CodeWarrior installation path or unable to write to it. Here are some possible situations:

  1. After CodeWarrior install, install path has been moved or renamed.
  2. CodeWarrior has been installed with administrator rights and it is run as normal user.
  3. CodeWarrrior install layout is somehow corrupted.

Workaround for each situation:

1.

A.

Close CodeWarrior.

Go to CodeWarrior_Install_Path\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\components\ and delete compreg.dat and xpti.dat files.

Open CodeWarrior.

Or

B.

Close CodeWarrior.

Go to CodeWarrior_Install_Path\eclipse\plugins\com.freescale.morpho.core_7.0.0.10-201507202206-g855a084\xpcom\bin\components\ and delete compreg.dat and xpti.dat files.

Run register_xpcom.bat.

2. Run 1.A. or 1.B. steps as administrator.

3. Reinstall CodeWarrior. Please note that if install has been somehow corrupted, uninstall might throw errors, in this case, it would be safer to manually delete CodeWarrrior install layout.

I understand you already run steps 1.B and 3 trying to fix the problem. Could you please make sure you have run steps as indicated above? Also if nothing above helps, could you please check if compreg.dat and xpti.dat files are created or not in your layout when you are performing above steps?

Regards,

Alexandra

Alexandra Arcalianu

Software Engineer, DevTech, Software Analysis

NXP Semiconductors

Phone: +40 021 305 2049

Email: alexandra.arcalianu@nxp.com

0 Kudos
Reply
3,239 Views
d_li
Contributor III

Hi Alexandra,

I have tried all the steps above as both admin/regular user. I have also tried installing to a different directory. Results are the same. Any other suggestions? Thanks,

-David

0 Kudos
Reply
3,239 Views
alexandraarcali
NXP Employee
NXP Employee

Hi David,

Here are some questions trying to localize your problem:

1. Do you still see this specific error "com.freescale.morpho.core.CWException: The function "getServiceByContractID" returned an error condition  (0x80040154)", right?

2. While performing above steps I gave you, have you seen compreg.dat and xpti.dat files at mentioned location? If you see then please send them to me.

3. What OS are you using? I've seen is Windows from errors above but just want to make sure is one of those recommended in release notes.

4. Have you installed in the past a CodeWarrior release prior to 10.9.0, e.g., 10.8.x, that has worked without errors on machine you have this problem for 10.9.0?

5. Do you see any errors while installing CodeWarrior? Do you have low disk space warnings while installing or running CodeWarrior?

6. Have you tried installing 10.9.0 CodeWarrior on other machine also?

Regards,

Alexandra

0 Kudos
Reply
3,239 Views
d_li
Contributor III

1) Yes. I see that specific error as shown in the image.

2) I will send you the 2 files.

3) Windows 7

4) I have used codewarrior 10.7, 10.8 and 10.5 without issues in the past

5) There are no visible warnings/errors while installing codewarrior. I have sufficient space.

6) Yes, I have installed codewarrior 10.9 w/o issues on another machine.

0 Kudos
Reply
3,238 Views
Anonymous
Deactivated User

Hi David,

can you please remove the below plug-in from CW installation directory and  check if the behavior change!!

<installation dir>\eclipse\plugins\com.freescale.sa_2.0.0.154851-201511241343

BR

Marc

0 Kudos
Reply
3,239 Views
d_li
Contributor III

Thank you Marc. Your suggestion has worked! :smileyhappy:

0 Kudos
Reply
3,239 Views
Anonymous
Deactivated User

Thx David, can you please  try this:

1- put back the plug-in

2- edit cwide-env located in <CWinstallation>\eclipse\cwide-env

3- add at the end of the file the below line:

PYTHONHOME= -add %CD%../SC/morpho_sa/bin/python

4- restart the IDE,

BR

Marc

0 Kudos
Reply
3,239 Views
d_li
Contributor III

Relevant error from .log in workspace

!ENTRY com.freescale.sa.analysispoints 4 120 2016-01-22 10:26:33.349

!MESSAGE Internal error

!STACK 0

com.freescale.morpho.core.CWException: The function "getServiceByContractID" returned an error condition  (0x80040154)

  at org.mozilla.xpcom.internal.XPCOMJavaProxyFSL.callXPCOMMethod(Native Method)

  at org.mozilla.xpcom.internal.XPCOMJavaProxyFSL.invoke(XPCOMJavaProxyFSL.java:143)

  at $Proxy7.getServiceByContractID(Unknown Source)

  at com.freescale.sa.analysispoints.TracepointManager.loadApManConfigs(TracepointManager.java:648)

  at com.freescale.sa.analysispoints.TracepointManager.loadExistingTracepoints(TracepointManager.java:187)

  at com.freescale.sa.analysispoints.TracepointManager.initialize(TracepointManager.java:53)

  at com.freescale.sa.analysispoints.Tracepoint.initManager(Tracepoint.java:1781)

  at com.freescale.sa.analysispoints.AnalysispointsPlugin.start(AnalysispointsPlugin.java:291)

  at org.eclipse.osgi.framework.internal.core.BundleContextImpl$1.run(BundleContextImpl.java:711)

  at java.security.AccessController.doPrivileged(Native Method)

  at org.eclipse.osgi.framework.internal.core.BundleContextImpl.startActivator(BundleContextImpl.java:702)

  at org.eclipse.osgi.framework.internal.core.BundleContextImpl.start(BundleContextImpl.java:683)

  at org.eclipse.osgi.framework.internal.core.BundleHost.startWorker(BundleHost.java:381)

  at org.eclipse.osgi.framework.internal.core.AbstractBundle.start(AbstractBundle.java:299)

  at org.eclipse.osgi.framework.util.SecureAction.start(SecureAction.java:440)

  at org.eclipse.osgi.internal.loader.BundleLoader.setLazyTrigger(BundleLoader.java:268)

  at org.eclipse.core.runtime.internal.adaptor.EclipseLazyStarter.postFindLocalClass(EclipseLazyStarter.java:107)

  at org.eclipse.osgi.baseadaptor.loader.ClasspathManager.findLocalClass(ClasspathManager.java:462)

  at org.eclipse.osgi.internal.baseadaptor.DefaultClassLoader.findLocalClass(DefaultClassLoader.java:216)

  at org.eclipse.osgi.internal.loader.BundleLoader.findLocalClass(BundleLoader.java:400)

  at org.eclipse.osgi.internal.loader.BundleLoader.findClassInternal(BundleLoader.java:476)

  at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:429)

  at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:417)

  at org.eclipse.osgi.internal.baseadaptor.DefaultClassLoader.loadClass(DefaultClassLoader.java:107)

  at java.lang.ClassLoader.loadClass(Unknown Source)

  at org.eclipse.osgi.internal.loader.BundleLoader.loadClass(BundleLoader.java:345)

  at org.eclipse.osgi.framework.internal.core.BundleHost.loadClass(BundleHost.java:229)

  at org.eclipse.osgi.framework.internal.core.AbstractBundle.loadClass(AbstractBundle.java:1207)

  at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:174)

  at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:905)

  at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:243)

  at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:55)

  at org.eclipse.ui.internal.WorkbenchPlugin$1.run(WorkbenchPlugin.java:268)

  at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:52)

  at org.eclipse.ui.internal.WorkbenchPlugin.createExtension(WorkbenchPlugin.java:264)

  at org.eclipse.ui.internal.EarlyStartupRunnable.getExecutableExtension(EarlyStartupRunnable.java:117)

  at org.eclipse.ui.internal.EarlyStartupRunnable.run(EarlyStartupRunnable.java:66)

  at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)

  at org.eclipse.ui.internal.Workbench$57.run(Workbench.java:2572)

  at org.eclipse.core.internal.jobs.Worker.run(Worker.java:54)

0 Kudos
Reply