t2081 codewarrior jtag issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

t2081 codewarrior jtag issue

Jump to solution
15,779 Views
sabeer
Contributor II

Hi NXP team and contributors,

I am using t2081 custom board and from codewarrior running bareboard project
when running the program initially I am getting an error
CCSprotocolPlugin: Failed to reset the target

[CCS last error: T2080: Core not responding]


help me in solving it

0 Kudos
Reply
1 Solution
15,286 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "4.3 Power-on reset recommendations" in https://www.nxp.com.cn/docs/en/application-note/AN4804.pdf

In addition, please make sure that you have configured the switch setting on your target board to make the target board booting from hard-coded RCW.

View solution in original post

0 Kudos
Reply
11 Replies
15,086 Views
sabeer
Contributor II

Dear Yipingwang,
thank you for your quick response,
it was a hardware issue which is fixed

0 Kudos
Reply
15,744 Views
yipingwang
NXP TechSupport
NXP TechSupport

It seems that there is no valid RCW on your custom board, please refer to "4.6.4.1.2 RCW Settings for Hard-Coded Options" in T2080RM.pdf to configure your target board as hard-coded RCW.

Then in CodeWarrior IDE, please create a SRAM launching project to connect to the target board to  avoid DDR controller initialization.

0 Kudos
Reply
15,685 Views
sabeer
Contributor II

Dear yipingwang,
now facing the issue,
CCSProtocolPlugin : Failed to correctly configure the JTAG chain.

i have tried using hardcoded rcw from t2080rm as well as default T2081 rcw file.

i am sharing the document of the steps followed for project creation and the error i am getting
Help me in resolving it.

0 Kudos
Reply
15,649 Views
yipingwang
NXP TechSupport
NXP TechSupport

In CodeWarrior IDE, please don't use JTAG configuration file to override RCW on the target board. Because the JTAG configuration is only used for the demo board, you need to customize it.

The simple way is to configure the switch settings on the custom board to configure the target board as hard-coded RCW. Then use CodeWarrior to connect to your custom board.

If your problem persists, please send the the following CCS commands result to me to do more investigation.

After configuring the target board as hardcoded RCW, and open the

CodeWarrior Connection Server from

C:\Freescale\CW_PA_v10.5.1\PA\ccs\bin\ccs.exe and type the following

commands.

(bin) 49 % delete all

(bin) 50 % config cc cwtap

(bin) 51 % show cc

0: CodeWarrior TAP (cwtap:10.193.20.66) CC software ver. {0.0}

(bin) 52 % ccs::config_chain t2080

(bin) 53 % ccs::reset_to_debug

0 Kudos
Reply
15,631 Views
sabeer
Contributor II

Dear Yipingwang,

below attached is the output image of the commands you shared.

0 Kudos
Reply
15,595 Views
sabeer
Contributor II

Hi yipingwang,

please find information regarding fpga reset logic,

kindly suggest us modifications if required.

0 Kudos
Reply
15,537 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "Figure 3. JTAG interface connection" in https://www.nxp.com.cn/docs/en/application-note/AN4804.pdf.

Please make sure you could get similar waveform as page 3 in the attached document.

0 Kudos
Reply
15,483 Views
sabeer
Contributor II

Dear Yipingwang,
thanks for your quick response,


we are still getting the error failed to correctly the jtag chain.

we cross verified your design with the ppt.

below attached are the images for reset sequences.

0 Kudos
Reply
15,389 Views
yipingwang
NXP TechSupport
NXP TechSupport

It seems that no problem with JTAG interface design.

Please refer to "Figure 4-1. Power-on reset sequence" in T2080RM.pdf to check the timing diagram of the POR sequence on your custom board.

0 Kudos
Reply
15,320 Views
sabeer
Contributor II

Dear yipingwang,

when powering on the processor Hrst is continously low, we have kept 4.7k pullup resistor at hrst pin still it is always low

our resets are connected to fpga, we tried driving hrst to high from fpga but the output is 1.1v

we have tried changing resistor values 1k and 75ohms but still same problem remains

kindly suggest us modifications

i am attaching a part of schematics relating to hrst

0 Kudos
Reply
15,287 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "4.3 Power-on reset recommendations" in https://www.nxp.com.cn/docs/en/application-note/AN4804.pdf

In addition, please make sure that you have configured the switch setting on your target board to make the target board booting from hard-coded RCW.

0 Kudos
Reply