some items of DDR configuration?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some items of DDR configuration?

2,871 Views
ybhao
Contributor I

1.png

1. my board SMT Memory Cell  directly, and  no spd eeprom , so i should select the discrete dram?

2. what's the difference between “DDR :200MHZ "  and " DDR date rate 400MT/s ",  the DDRCLK is set to  400MHZ by starpping pin, the uboot message is right?

 i think it should be print “DDR : 400MHZ” and " DDR date rate 800MT/s ",so this is uboot bug?

3. i don't see the " DDR date rate 400MT/s " in QCVS ddr configuration tabs, why?

4. clk to DQS skews, ----- is the Length difference ? 

abs(DQS0 of length - (CLK_cpu to CLK_ic1 of length))

 abs(DQS1 of length - (CLK_cpu to CLK_ic1 of length))

abs(DQS2 of length - (CLK_cpu to CLK_ic2 of length))

abs(DQS3 of length - (CLK_cpu to CLK_ic2 of length))

abs(DQS4 of length - (CLK_cpu to CLK_ic3 of length))

abs(DQS5 of length - (CLK_cpu to CLK_ic3 of length))

abs(DQS6 of length - (CLK_cpu to CLK_ic4 of length))

abs(DQS7 of length - (CLK_cpu to CLK_ic4 of length))

 

thank you very much !

 

0 Kudos
Reply
7 Replies

2,855 Views
ybhao
Contributor I

1.png

1. does i can use the timing of above as default init value  before learning ?  if not ,  which critical param should i set , have some document?

2.png

2. which script sould i run?

 

3.png

 

now i can find cwtaps at ccs, and can connect chip at debug mode.  but  at QCVS mode ,i can't connect , thank you

0 Kudos
Reply

2,819 Views
ybhao
Contributor I

thank you very much!

1.png

1.  does the timing of above can be use default value before learning cycle ?  if not, which  Critical parameter  should i set,have some document  to reference?

 

 

2.png

2.  all the script of the above should be run?

3.png

 

i can find my cwtaps at ccs, but i can‘t connect chip at QCVS ,  help me,  and i   can connect chip at debug mode now。

thanks

0 Kudos
Reply

2,864 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. You could select discrete dram.

2. u-boot is correct, DDR clock frequency is 66.66/2*6=200MHz, data rate is 400MT/s.

3. Please create a QCVS DDR project, then double click "DDR_mc1:DDR" component to show Properties panel, you could configure "DDR Bus Clock" as 200MHz in the Properties panel.

4. The Length is different.

2,824 Views
ybhao
Contributor I

4.png

why uboot print ddr clk  should div 2?   

0 Kudos
Reply

2,826 Views
ybhao
Contributor I

can you tell me ,  66.66/2*6=200MHz,    div 2 , where i can see the div 2 ?  thank you very much

0 Kudos
Reply

2,816 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the section "System clock and DDR controller clock" in P2020 Reference Manual.

If further discussion is needed, please create new a thread in https://community.nxp.com/t5/QorIQ/bd-p/qoriq-grl, the hardware team will help to explain more.

0 Kudos
Reply

2,853 Views
ybhao
Contributor I
0 Kudos
Reply