ethernet tap netparam

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethernet tap netparam

Jump to solution
1,550 Views
iv
Contributor I

Hi,

i'm working on CW with ethernet tap rev b on target p3041.

I did a wrong command with netparam on telnet shell ("netparam bootconfig static") without ip and now the tap is unreachable.
Is it possible to rectify this parameter?

thks
Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,416 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
1,416 Views
iv
Contributor I

ok thanks,i used screen on /dev/ttyACM0.

0 Kudos
Reply
1,417 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

0 Kudos
Reply