V10 - Coldfire -  I can't open a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

V10 - Coldfire -  I can't open a project

720 Views
MichaelEdwards
Contributor I

I am new to V10 and programming for coldfire.  I am runnning special edtion.

Why can I NOT do a simple Open Project. From the menu Project>>Open Project.

It is greyed out.

 

Thanks in advance.

Labels (1)
0 Kudos
2 Replies

325 Views
CrasyCat
Specialist III

Hello

 

Are you looking for a way to add an existing project to your workspace?

If this is what you are looking for you need to use File > Import and then select General > Existing Project into Workspace.

 

The entry Project > Open Project can only be used for project that are already visible in the Workspace, but have be closed (using Close Project).

 

CrasyCat

0 Kudos

325 Views
MichaelEdwards
Contributor I

I'll try that. Thanks

0 Kudos