Hi,
I'm trying to install CodeWarrior on my 64bit Ubuntu 14.04.
I get the following error.
Please read the information below.
The following dependecies are required to run CodeWarrior for PA :
32 Bit versions of these libraries are required:
libstdc++.so.6[OK] libexpat.so.0/so.1[NOT FOUND]
For a detailed guide on obtaining the required libraries please refer to the
README.txt document that was delivered alongside this installer.
Press Next to refresh this screen or continue.
Note: the tools will not install correctly without these prerequisites which
are used during the installation process. Advanced users can restart the
installer with the -V SKIPLIBS=1 flag to disable this check.
I did
sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0s
sudo apt-get install bc
sudo apt-get install lib32stdc++6
But I still see the same error.
Where can I pick up the correct libraries?
Thanks
Uday
解決済! 解決策の投稿を見る。
Hello Uday,
Please install package libexpat1 first, then install CodeWarrior.
sudo apt-get install libexpat1-dev:i386
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Uday,
Please install package libexpat1 first, then install CodeWarrior.
sudo apt-get install libexpat1-dev:i386
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for this help. It installed successfully.
However I'm unable to run cwide after installation. No error messages are seen. I do see it fails with value 13 though.
Thanks
Uday
Refer to README.txt from installation kit and follow the steps for Ubuntu 13.10 64bit.
2.14 Ubuntu 13.10 64bit:
1) Install OS with default settings.
2) Open Terminal and run
# sudo apt-get install libc6:i386 libgcc1:i386 gcc-4.6-base:i386 libstdc++5:i386 libstdc++6:i386 libgtk2.0-0:i386 libxpm4:i386 libusb-0.1-4:i386 libusb-1.0-0:i386 libuuid1:i386 libxcb1:i386 libnspr4:i386 libglib2.0-0:i386 libxdamage1:i386 libxtst6:i386
3) Install CodeWarrior.
Perfect.
Its working now. Thanks for pointing out the relevant section. I missed that in the readme.
Regards
Uday