Some elements of GUI dialogs not seen in CW 10.3 for PA (QorIQ)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some elements of GUI dialogs not seen in CW 10.3 for PA (QorIQ)

Jump to solution
1,678 Views
kanatalimzhanov
Contributor III

Hello,

It seems to be issue of my host operating system.

I can not see some elements of CW dialogs.

Here is two screen shots:

kanat@kanat:~/work/u-boot/CW10.3$ ls *jpg

Reset_Screen_of_CW_10_3__.jpg  Target_properties_screen_of_CW_10_3__.jpg

kanat@kanat:~/work/u-boot/CW10.3$

16894_16894.jpgReset_Screen_of_CW_10_3__.jpg

 

16895_16895.jpgTarget_properties_screen_of_CW_10_3__.jpg

 

And my host operating system info:

 

kanat@kanat:~/work/u-boot/CW10.3$ uname -a

Linux kanat 3.2.0-37-generic-pae #58-Ubuntu SMP Thu Jan 24 15:51:02 UTC 2013 i686 i686 i386 GNU/Linux

kanat@kanat:~/work/u-boot/CW10.3$ lsb_release -d

Description:    Ubuntu 12.04.5 LTS

kanat@kanat:~/work/u-boot/CW10.3$

 

I have seen same behavior in Demo version of CodeWarrior 10.4.0 for PA.

What can i do to see GUI elements better?

Thanks for help in advance.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,419 Views
catalindemergia
Contributor IV

Hello,

the "echo $XDG_CURRENT_DESKTOP" command returns "Unity", which is a graphical shell for the

GNOME desktop environment.

regards,

Catalin

View solution in original post

0 Kudos
Reply
12 Replies
1,419 Views
catalindemergia
Contributor IV

Hello,

I installed CW PA 10.3 on my "Ubuntu 12.04.4 LTS" system.

The commands I ran in order to install CW were

sudo apt-get install ia32-libs

sudo apt-get install bc

./setuplinux

I took these instructions from the 2.12 section in README.txt.

I could see the checkboxes without doing any other changes.

screen.png

regards,

Catalin

1,419 Views
kanatalimzhanov
Contributor III

Thanks Yiping Wang and lunminliang.

Thanks, Catalin.

Which desktop you are using? KDE or GNOME ?

I will try this way also

"sudo apt-get install ia32-libs

sudo apt-get install bc

./setuplinux

"

Meantime checked that in GNOME desktop of Ubuntu 12.04  CW 10.3 dialogs shown correct.

GNOME_Target_properties_screen_of_CW_10_3__.jpg

0 Kudos
Reply
1,420 Views
catalindemergia
Contributor IV

Hello,

the "echo $XDG_CURRENT_DESKTOP" command returns "Unity", which is a graphical shell for the

GNOME desktop environment.

regards,

Catalin

0 Kudos
Reply
1,419 Views
lunminliang
NXP Employee
NXP Employee

I am using CW10.3.3 on Ubuntu 14.04 and do not have problem. Have you installed those dependancy as in install_deps.sh?

See mine:

freescale@freescale-sdk:~$ uname -a

Linux freescale-sdk 3.13.0-24-generic #46-Ubuntu SMP Thu Apr 10 19:08:14 UTC 2014 i686 i686 i686 GNU/Linux

freescale@freescale-sdk:~$ lsb_release -d

Description:    Ubuntu 14.04 LTS

freescale@freescale-sdk:~$

pastedImage_2.png

1,419 Views
kanatalimzhanov
Contributor III

Can not find this file, "install_deps.sh".

In file README.txt no special instructions about Ubuntu

"2.2 Ubuntu 8.04 32bit installation procedure:

   1) Install OS with default settings.

   2) Install CodeWarrior. No dependencies are required.

"

No words about Ubuntu 12.04 or 14.04

Can you be so please to post that file (install_deps.sh) here?

0 Kudos
Reply
1,419 Views
lunminliang
NXP Employee
NXP Employee

On my host, the file is right under the CW installation directory.

freescale@freescale-sdk:/opt/Freescale/CodeWarrior_PA_10.3.3$ ls

Cross_Tools  eclipse  install_deps.sh  PA      restore.pl

detect.sh    gnu      jre              remove  uninstall

0 Kudos
Reply
1,419 Views
kanatalimzhanov
Contributor III

I think that you have CW 10.3.3 version (and mine 10.3) make a difference.

Mine here:

kanat@kanat:/opt/Freescale/CodeWarrior_PA_10.3$ ls

Cross_Tools  eclipse  gnu  _jvm  PA  _uninst

Maybe here is a way to upgrade from CW 10.300 to 10.3.3 ?

I found a workaround for this little inconvenience:

*) when Target_properties_Dialog or Reset_Dialog appears one may scroll-unscroll cores list (where e500mc-0 ... e500mc-7 listed)

   after this elements of GUI seen much better. Here is a picture.

Reset_Screen_of_CW_10_3__.jpg

0 Kudos
Reply
1,419 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kanat Alimzhanov,


If the eclipse plugin cannot be displayed correctly on Ubuntu OS, there is a workaround would be helpful for you.

Please change the appearance from System->Preference->Appearance, and select "clearlooks".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,419 Views
kanatalimzhanov
Contributor III

I have a try on my Ubuntu

kanat@kanat:~/P4080DS/Uboot$ uname -a

Linux kanat 3.2.0-37-generic-pae #58-Ubuntu SMP Thu Jan 24 15:51:02 UTC 2013 i686 i686 i386 GNU/Linux

kanat@kanat:~/P4080DS/Uboot$ lsb_release -d

Description:    Ubuntu 12.04.5 LTS

kanat@kanat:~/P4080DS/Uboot$

Next steps:

Settings --> System_settings --> Application_appearance --> Style --> Widget_style -->  change from "Oxygen" to "clearlooks".

A lot of changes in appearance of windows but no help to resolve my problem.

README file of CW 10.3  say that CW works on Ubuntu with default settings.

Maybe i should use default desktop system of ubuntu GNOME instead of KDE?

(now i use KDE desktop).

I will try to install GNOME desktop and write here about results.

0 Kudos
Reply
1,419 Views
lunminliang
NXP Employee
NXP Employee

Thanks for sharing.

Maybe here is a way to upgrade from CW 10.300 to 10.3.3 ?

> I think you need to install from the new installer.

0 Kudos
Reply
1,419 Views
kanatalimzhanov
Contributor III

"Have you installed those dependancy as in install_deps.sh?"

I am unsure. Remember that installed something like when start to use QCS (QorIQ Configuration Suite).

I will recheck, and maybe upgrade my Ubuntu.

Thanks.

0 Kudos
Reply
1,419 Views
lunminliang
NXP Employee
NXP Employee

In my impression, when I was installing CodeWarrior, it tells the dependency has already been installed successfully.

0 Kudos
Reply