Small bug in CW 7.1.1 for ColdFire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Small bug in CW 7.1.1 for ColdFire

1,527 Views
MrBean
Contributor I
In the project settings -> Code generation -> Global optimizations
there is a field "Use .sdata/.sbss for" -> "All data smaller than" (number field)
 
I've set this (number field) to 4
 
This results in all data smaller or equal to 4 bytes be put in .sdata/.sbss
Setting the field to "3" solves it.
 
But... imho 4 is not smaller than 4  :smileywink:
 
Labels (1)
0 Kudos
Reply
1 Reply

582 Views
CrasyCat
Specialist III
Hello
 
I would recommend you to submit a service request for that to make sure we get that addressed..

Click here to submit a service request.

CrasyCat
0 Kudos
Reply