SLOW IO using BDM Console IO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SLOW IO using BDM Console IO

1,852 Views
mredekopp
Contributor I

Hi,

 

I know there were a couple threads about this a year or two back, but I'm experiencing VERY VERY SLOW console I/O with printf (a few chars per sec.) with the MCF 5211 and MCF52295.  I'm using Codewarrior 7.1 (build 2502).

 

Can you tell me where in the library and/or header files to re-enable buffered (by line) I/O rather than by character.  Any solutions at all.  This is kind of a make-it-or-break-it issue as I'm using it in the classroom and students need debug capabilities that are faster...

 

Thanks,

Mark

Labels (1)
0 Kudos
Reply
1 Reply

1,166 Views
J2MEJediMaster
Specialist I

I remember that thread, and its information was placed into a FAQ for this kind of situation. FAQ-28993 describes how to set up console I/O via BDM, and how to buffer it by line rather than character to improve output performance. Type "FAQ-28993" into the Enter Keyword box at the upper right of this web page and the search system should take you to it. HTH.

 

---Tom

 

0 Kudos
Reply