Re: CodeWarrior 10.5 for Power Arch with QCVS
I'm using the DDR Configuration tool from QCVS to configure for DDR3L.
I'm trying to add config for extended temperature self-refresh (ASR/SRT). My MR2 value (SDRAM_MODE_2) is always zero. Where do I configure for self-refresh?
Also, how is DDR_SDRAM_INTERVAL calculated? My device datasheet (IS46TR16128DL) specifies a refresh interval of 8K cycles. How do I achieve this?
Thanks
Solved! Go to Solution.
In Properties panel in QCVS DDR tool, please click "Advanced" at the right top of the panel, then go to "SDRAM Mode Configurations"->"SDRAM mode 2(MR2) - DDR SDRAM. Please refer to my screenshot as the following.
In Properties panel in QCVS DDR tool, please click "Advanced" at the right top of the panel, then go to "SDRAM Mode Configurations"->"SDRAM mode 2(MR2) - DDR SDRAM. Please refer to my screenshot as the following.