Problems when CodeWarrior flash u-boot to P2020RDB-PCA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems when CodeWarrior flash u-boot to P2020RDB-PCA

跳至解决方案
2,439 次查看
baijack
Contributor II

Hi there.

We accidentally got uboot erasred from our p2020rdb-pca board.

And we got a CodeWarrior USB TAP, so we flash the uboot.bin file to p2020rdb-pca by codewarrior.

We follow the steps in cheatsheet but in the end we got a error as the image below:

6307_6307.jpgerror.jpg

It says Core not responding, is there any problem with our board or we dont do it right on software?

Thx.

标签 (1)
1 解答
1,952 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

3. You can make directly the connect target from GUI. Basically, this will only run the tcl initialization file on the target (no application is made/built or downloaded).

P2020RDB_ConnectTarget.png

4. This is not so good. The ASLEEP led should be ON only during reset operation, just after that this should be OFF. Please try and the attached jed file for CPLD and let me know the results.

Regards,

Marius

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,952 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

1. What CW version are you using?

2. Did you make a P2020RDB-PC project?

3. Please use the connect target and the default P2020RDB-PC flash programmer target task.

4. Please double-check the DIP SW settings to be according with the ones from README file.

Let me know the results,

Marius

0 项奖励
回复
1,952 次查看
baijack
Contributor II

Hi,

Thanks for your reply.

   1. The CW version is 10.3

   2. Yes,we did.

   3. We don't know what do you mean about the "connect target"

   4. We checked the SW settings and reflash the CPLD JED file.

     There seems to have some new problem, the ASLEEP LED is on and we got a new error, display as below:

aaaaa.jpg

It seems that p2020 is on sleep mode, how can we wake it up? or there is other reason for this?

Thx again.

0 项奖励
回复
1,953 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

3. You can make directly the connect target from GUI. Basically, this will only run the tcl initialization file on the target (no application is made/built or downloaded).

P2020RDB_ConnectTarget.png

4. This is not so good. The ASLEEP led should be ON only during reset operation, just after that this should be OFF. Please try and the attached jed file for CPLD and let me know the results.

Regards,

Marius

0 项奖励
回复
1,952 次查看
baijack
Contributor II

Hi,

Thanks for your reply.

3. We did as you showed but still the same error.

4. The jed file you attached can't be flashed, says ' The data file may not be valid for the device selected.'

     The jed file we used before is p1021combo_rev4.1.jed, and that is fine to flash.

Regards,

Bai

0 项奖励
回复
1,952 次查看
marius_grigoras
NXP Employee
NXP Employee

So, indeed seems to be a hardware issue regarding your custom board. You can check the steps suggested by Heinz here [1].

Regards,

Marius

[1] https://community.freescale.com/message/351886?et=watches.email.thread#351886

0 项奖励
回复