Nxp P2020 how much current will consume it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nxp P2020 how much current will consume it

490 Views
nareshpuli
Contributor III

Hi,

we are using  P2020RDB Board, The supply is  12V, 5V how much current it will consume it, how much current CPU consume to bring up the Board

Regards

Naresh

0 Kudos
1 Reply

292 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, board designers do not specify full power consumption of entire board in board documentation.

I can only specify power supply type (and parameters) we use with our board.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos