Need help in bringing up the board with MPC5200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help in bringing up the board with MPC5200

1,056 Views
Sam_D
Contributor I

Hi,

 

Can some one tell me the details I should be considering while bringing up the target like the what are the files and things I am suppose to look into.

 

I have a vague idea about the make file and .lcf file changes.

 

Kindly help me out with this. An over view of the changes in general dat i can expect.

Labels (1)
0 Kudos
Reply
1 Reply

602 Views
J2MEJediMaster
Specialist I
Check out FAQ-27855. Although it discusses writing a configuration word into flash for a prototype board, the directions for configuring the CodeWarrior debugger to work with the prototype board apply here. Be sure the read the supporting documentation this FAQ mentions. Good luck.
0 Kudos
Reply