MPC8349 - CW download linux to target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8349 - CW download linux to target

1,764 Views
steverino2
Contributor I
:manhappy:
 
Hi all, well I'm continuing down the path building Linux for mpc8349 PPC.
 
So far I have been unable to get USBTAP to work directly connected to my Linux
build machine.   BUT as a workaround I'm using a Windows PC for a connection server.
 
I've worked out a toolchain that is now coming to life
 
 
CW Dev Studio          Code Warrior Pro                                       MPC8349
Linux FC6                   Windows XP              <-- USB TAP --->    target
build machine             Connection Server
             |--------  LAN -------------|
      
 
The build machine uses external makefile to build linux.  Then from Code Warrior
I load vmlinux and halt the target system via the Windows CCS.  So far so good.
 
Now the question:  How can I get vmlinux to download to the target?  When the
Code Warrior session comes up on the build machine, it loads the vmlinux
binary and catalogs the source files, BUT doesn't seem to want to download the
binary to the target.
 
I'd appreciate any advice from anyone who might be working in a similar project.
 
/steverino2
 
 
Build Machine Host:  Linux FC6
target:  MPC8349E-mITX
CW Linux:  Code Warrior Development Studio for Power PC, Linux Platform Edition v8.7


--
Alban Edit: Please always include FSL Part Number in Message Subject line.



Message Edited by Alban on 2007-09-07 03:04 PM
Labels (1)
0 Kudos
Reply
1 Reply

650 Views
Black
Contributor I

This should work if it is done from the Linux machine on which the USP TAP is connected. I don't think using the Windows machine for CCS connection is such a good idea. I think it should be fixed the problem why the USB TAP is not working on the Linux machine.

If this USB TAP connection issue is still not resolved, please submit a service request for this issue at:

https://www.freescale.com/webapp/servicerequest.create_SR.framework

Thanks,

D

0 Kudos
Reply